Chalk Lines

A Chalk line or also known as a Chalk box is a simple hand tool that consists of a box filled with chalk powder with a reel of string inside it. The chalk lines are a tool for marking long, straight lines over distances onto the surface of an object to provide accurate guides where using a ruler or straight edge tool would be impractical. On the end of the chalk powdered string is a metal hook which can be attached to an object at one end and then reeled out across the surface and pulled taut. Once the chalk string line is in the correct position it can be plucked at its centre and the tension in the string will make it snap back down and create a chalk line on the surface of your object. Chalk lines are typically used to mark lines on relatively flat surfaces. This chalk line tool provides accurate guides prior to cutting, laying tiles, levelling posts, handing wallpaper and many other tasks and is mostly used in carpentry.

...
Read more Read less

Filter

Visar 1 - 1 av 1 produkter
Resultat per sida
Beskrivning Pris Line Material Length Supplied With
RS-artikelnummer 269-4310
Tillv. art.nrT3520B
VarumärkeCK
135,46 kr
Each
Enheter
- 30m Chalk refill